Other Parts Discussed in Thread: PLLATINUMSIM-SW
Hello together,
I was wondering, if the input signal at OSCin (PIN 8/9) is a square wave signal, might improve the spurs in the frequency domain in the region from 0 Hz -> f_Lo.
I did read in the data sheet (if I understood it correctly) that the slewrate of the input signal is directly related to quality of the frequency domain output.
Is this related to the integer devider?
Thank you for your time. :-)