Part Number: CDC2351
Other Parts Discussed in Thread: LMK00101
Team,
I was looking at the logic level output and was noticing that typically u want 2.4V or so going into a device that wants 2V min…
This is 2V but the test condition was 3V instead of 3.3V.. So would it be higher at 3.3V?
2V and 0.8V are right at the levels where I have 0 margin…