Part Number: CDCE6214-Q1
Other Parts Discussed in Thread: USB2ANY,
Hello,
I am trying to program the CDCE6214-Q1 EEPROM using TICSPRO GUI and USB2ANY, with my application specific settings of CDCE6214-Q1 while in Serial Interface Mode. I am using a .tcs file with the mentioned settings, and load this prior to any EEPROM write attempt. However, when I follow steps 1-8 in CDCE6214-Q1 datasheet section 10.5.2.3.1, using Register Commit Flow method and confirming register write/read statuses in the prompt with each step, the read back register values after completing all steps are the default values still, and not my settings/values.
I have also considered that the steps include the hex values, and the values to be written in the GUI are in decimal, and that the some steps are most easily and confidently done in the 'User Control' page and the EEPROM reg commit operation is done on the 'EEPROM' page. I have also tried the steps using the 'User Control' page with no success.
Schematically, REF_SEL is grounded through 4.7 k ohm, and HW_SW_CTRL is pulled high to 1.8V (VDD for CDC is 1.8V) through 4.7k ohm res. The CDCE6214-Q1 is at 0x68.
What might I be missing here?