Hello,
My LMK05318's Two Reference Clock Inputs are 1pps and output5 is 1.8V CMOS 10Mhz, if two inputs lost and LMK05318 will be holdover mode, then the 10MHz output holdover stability will depend on external TCXO.
My question is if in holdover mode,output clock needs meet Stratum 3/3E,then must my TCXO use high accuracy TCXO,for example Stratum 3/3E TCXO or TCXO can use common device,for example +/- 0.5ppm TCXO?
Thanks.