This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594EVM: LMX2594EVM Phase noise

Part Number: LMX2594EVM
Other Parts Discussed in Thread: LMX2594

Hi All, 

 I'm checking the possibility of an external clock source (instead of XTAL) for feeding the clock to our test board

I wish to request some information on LMX EVM 
 
  1. Does the EVM include clock source, power, SPI programming?
  2. Do we need anything non-standard for using this  ?
  3. How much is the amplitude of output (we need 1.8Vp-p for our clock-in)
  4. Any specific points to be taken care with Single-ended Vs Differential clock in input or output ?
  5. Does the EVM output expect 50Ohm termination on board?
  6. What is the frequency output programmable range from the module (we need 20M to 1G output)?

regards 

  • Hello,

    There is a REFERENCE PRO provided in the kit for clock source and programming as shown in figure 1.  You will need external power supply.

    1.8Vpp output can be provided with an inductor pullup although for higher frequencies the specification is usually in terms of dBm.

    The EVM is expecting external load of 50 ohms on the RF outputs. If not using the complimentary output it is recommended also to terminate the unused port with 50 ohms.

    The EVM output frequency range is compatible with the device 10 MHz to 15 GHz.

    The connections are standard SMA type

    Regards,

  • Thanks for the reply Liam, 

    for 1.8v output what is the typical inductor value that you suggest as as pullup?

  • Thanks for the reply Liam, 

    1. Can I assume the reference pro board comes along by-default with the clock module if I purchase it from the below link ?

    https://www.digikey.com/product-detail/en/texas-instruments/LMX2594EVM/296-46575-ND/7056941

    2. The serial connector cable between Pro and EVM also comes along  with LMX2594EVM ?

    3. Can you please suggest an exact part no for 100M Wenzel Oscillator that is suggested to be used in the TI document ?

    4. For 1.8v output what is the typical inductor value that you suggest as as pullup?

    regards 

  • Hi Siddharth,

    The box includes the LMX EVM, a Ref Pro board, a ribbon cable and a USB cable.

    The Wenzel clock is 501-4623G.

    1.8Vpp = 9.08dBm. From Figure 18 of the datasheet, you may not be able to get this voltage swing across all frequencies. Maybe you should consider to add an amplifier after LMX2594 in order to ensure that you can get sufficient signal swing to drive the next stage.

  • Thanks a ton ! for the reply Noel. 

    1. The 3.3V supply is fed-in through SMA, is there any alternate way to feed the supply ?

    2. For 1.8v output what is the typical inductor value that you suggest as as pullup?

  • Hi Siddharth,

    1. you can solder wires to the pads of the Vcc SMA connector. 

    2. We used 1nH inductor when taking data for Figure 18.

  • Thanks for the reply Noel,

    The required frequency range is 100 to 200 Mhz , I hope in this range the EVM can give 9.08dBm (1.8Vpp) swing ?

  • Hi Siddharth,

    Unfortunately, at 100MHz to 200MHz, the output voltage swing will drop to below around 1Vpp. 

    Are these the only frequencies you want? Will you consider clock generator instead of RF synthesizer? 

    This is the portfolio our clock generator. You can pick those clock generators with CMOS output to ensure you have greater than 1.8Vpp voltage swing.

    https://www.ti.com/clocks-timing/generators/overview.html

  • thanks for the reply Noel. I asked this range because I wasn’t able to figure that out from the plot , is this 1Vpp for 100-200Mhz mentioned somewhere?

    We wish to be able to have a reference which is programmable especially for testing PLL locking.

    The Wenzel part no. also doesn't appear to be available on digikey etc.. ?

  • Hi Siddharth,

    very often, we test the output at 100MHz, so we know the voltage swing. It is not mentioned in the datasheet.

    We have been using the Wenzel clock for many years, maybe it is already discontinued. 

    Here is the phase noise of the wenzel clock, FYI.

    100	-137.8524537
    101.8009751	-137.8992682
    103.6343854	-137.3426016
    105.5008148	-137.385904
    107.4008583	-136.842424
    109.335121	-136.8824657
    111.3042193	-137.6846404
    113.3087806	-137.7216588
    115.3494436	-136.4056712
    117.4268583	-136.4398895
    119.5416868	-138.5674836
    121.6946029	-138.7751949
    123.8862924	-138.809153
    126.1174537	-136.5436701
    128.3887977	-136.5717734
    130.701048	-139.192094
    133.0549413	-139.9679253
    135.4512277	-139.9929001
    137.8906706	-142.6719599
    140.3740473	-143.1823123
    142.9021489	-143.2045121
    145.4757811	-142.2143914
    148.0957637	-138.6123867
    150.7629316	-138.6321267
    153.4781344	-136.560729
    156.2422375	-140.6216759
    159.0561213	-139.2055194
    161.9206824	-139.2224096
    164.8368336	-138.720741
    167.805504	-141.034432
    170.8276394	-141.209088
    173.9042027	-141.3196402
    177.0361741	-141.503374
    180.2245515	-138.6664167
    183.4703509	-139.9914953
    186.7746062	-141.7124403
    190.1383704	-142.8787586
    193.5627151	-143.0565817
    197.0487315	-143.2240221
    200.5975301	-147.3227738
    204.2102417	-146.8500893
    207.8880174	-145.5261086
    211.6320288	-146.0728011
    215.443469	-145.2900807
    219.3235523	-147.3307789
    223.2735149	-146.2071403
    227.2946153	-144.4819937
    231.3881348	-142.9398046
    235.5553775	-142.7386586
    239.7976713	-143.4647049
    244.1163677	-144.9481308
    248.5128427	-144.8693751
    252.9884972	-145.1196955
    257.544757	-145.1688316
    262.183074	-145.1817491
    266.904926	-147.9539625
    271.7118173	-148.2611015
    276.6052795	-145.1922459
    281.5868718	-147.9194226
    286.6581812	-146.0248177
    291.8208238	-141.9798762
    297.0764442	-142.5608482
    302.426717	-144.4197824
    307.873347	-147.1046591
    313.4180693	-145.5613477
    319.0626508	-145.381531
    324.8088897	-143.689732
    330.658617	-144.2170927
    336.6136964	-146.4140371
    342.6760253	-146.4703616
    348.8475353	-149.3180422
    355.1301926	-145.311761
    361.525999	-147.4740912
    368.0369923	-146.5387762
    374.665247	-146.0114064
    381.4128748	-145.5054356
    388.2820258	-148.3233393
    395.2748885	-151.450274
    402.3936909	-153.29948
    409.6407011	-149.1022377
    417.0182282	-148.6992647
    424.5286227	-153.090505
    432.1742776	-149.9988315
    439.9576288	-150.1799065
    447.8811562	-149.6581912
    455.9473844	-151.9181173
    464.1588834	-148.7013797
    472.5182694	-153.072969
    481.0282058	-151.0901984
    489.6914041	-151.0332441
    498.5106245	-151.2570376
    507.4886768	-153.2057881
    516.6284216	-151.8854035
    525.9327709	-151.515451
    535.4046892	-151.6445633
    545.0471945	-151.7982895
    554.8633588	-153.192145
    564.8563098	-152.2280341
    575.0292314	-149.2416505
    585.3853648	-152.5621581
    595.9280096	-153.8019022
    606.6605248	-152.8866209
    617.5863299	-152.9538812
    628.708906	-151.6480723
    640.031797	-153.1317686
    651.5586104	-153.2729177
    663.2930188	-154.4795465
    675.238761	-155.1645858
    687.3996431	-156.2924817
    699.7795397	-154.5425356
    712.382395	-154.1861151
    725.2122247	-154.4140599
    738.2731164	-152.8183598
    751.5692316	-155.6597202
    765.1048064	-152.9576201
    778.8841536	-154.4939407
    792.9116634	-155.5374858
    807.1918052	-157.4696209
    821.7291288	-153.5248082
    836.5282659	-159.5017454
    851.5939318	-154.3210277
    866.9309266	-155.0245848
    882.5441369	-152.0980113
    898.4385372	-152.6192466
    914.6191917	-152.2410076
    931.0912558	-154.5249772
    947.8599777	-158.4137783
    964.9307	-155.663767
    982.3088618	-155.6340949
    1000	-157.2486947
    1018.009751	-156.0594829
    1036.343854	-155.6886807
    1055.008148	-153.3746483
    1074.008583	-156.2439014
    1093.35121	-154.7050021
    1113.042193	-158.2902283
    1133.087806	-158.0097788
    1153.494436	-158.3087275
    1174.268583	-156.8465076
    1195.416868	-155.6257909
    1216.946029	-158.0959909
    1238.862924	-157.9448176
    1261.174537	-158.2474333
    1283.887977	-157.3526361
    1307.01048	-157.9886868
    1330.549413	-158.8658716
    1354.512277	-160.9928731
    1378.906706	-157.0803825
    1403.740473	-162.213173
    1429.021489	-158.3551139
    1454.757811	-159.391963
    1480.957637	-160.2646632
    1507.629316	-157.6068662
    1534.781344	-159.8210664
    1562.422375	-159.512021
    1590.561213	-159.7119718
    1619.206824	-160.0839759
    1648.368336	-157.7309921
    1678.05504	-160.6468879
    1708.276394	-160.3411706
    1739.042027	-161.1580195
    1770.361741	-162.1044417
    1802.245515	-161.5188633
    1834.703509	-161.4943212
    1867.746062	-159.7020589
    1901.383704	-160.5858172
    1935.627151	-161.4468517
    1970.487315	-159.2654695
    2005.975301	-160.6655006
    2042.102417	-158.949612
    2078.880174	-160.5877005
    2116.320288	-160.9906314
    2154.43469	-159.3551751
    2193.235523	-160.2724937
    2232.735149	-160.0796857
    2272.946153	-161.0610351
    2313.881348	-161.6753493
    2355.553775	-160.6420156
    2397.976713	-161.432412
    2441.163677	-160.334978
    2485.128427	-161.4877766
    2529.884972	-161.9709806
    2575.44757	-160.8082343
    2621.83074	-160.3789833
    2669.04926	-161.7247656
    2717.118173	-161.3186798
    2766.052795	-161.0059243
    2815.868718	-162.5107034
    2866.581812	-160.1708421
    2918.208238	-160.7840016
    2970.764442	-161.8757629
    3024.26717	-160.6046149
    3078.73347	-160.9059018
    3134.180693	-162.6448201
    3190.626508	-162.8823862
    3248.088897	-161.350625
    3306.58617	-161.573322
    3366.136964	-162.3846326
    3426.760253	-162.1459585
    3488.475353	-162.1683777
    3551.301926	-161.7402896
    3615.25999	-161.9454149
    3680.369923	-161.5565565
    3746.65247	-162.0254695
    3814.128748	-160.9432636
    3882.820258	-160.724425
    3952.748885	-163.2357749
    4023.936909	-161.1807209
    4096.407011	-163.965115
    4170.182282	-162.1959797
    4245.286227	-160.0102769
    4321.742776	-161.5845675
    4399.576288	-162.913012
    4478.811562	-162.2834883
    4559.473844	-162.8176915
    4641.588834	-161.8600597
    4725.182694	-160.765818
    4810.282058	-161.4665292
    4896.914041	-161.1295533
    4985.106245	-161.5056677
    5074.886768	-161.7271199
    5166.284216	-161.1539879
    5259.327709	-161.5498316
    5354.046892	-162.8873787
    5450.471945	-163.2248621
    5548.633588	-161.2111258
    5648.563098	-161.9027911
    5750.292314	-160.4883916
    5853.853648	-161.064221
    5959.280096	-162.3405633
    6066.605248	-160.2661991
    6175.863299	-162.3986809
    6287.08906	-160.3820972
    6400.31797	-163.3628195
    6515.586104	-162.9897263
    6632.930188	-162.7826963
    6752.38761	-162.7906237
    6873.996431	-162.1238067
    6997.795397	-159.9424668
    7123.82395	-162.1341596
    7252.122247	-161.3497902
    7382.731164	-161.7964114
    7515.692316	-161.0447031
    7651.048064	-161.4738973
    7788.841536	-161.4582342
    7929.116634	-161.9973892
    8071.918052	-161.9261587
    8217.291288	-161.9035139
    8365.282659	-161.5098027
    8515.939318	-161.6787696
    8669.309266	-163.9846549
    8825.441369	-162.5636239
    8984.385372	-161.4323287
    9146.191917	-163.0241983
    9310.912558	-162.2935458
    9478.599777	-162.7343983
    9649.307	-161.2868552
    9823.088618	-162.9962368
    10000	-160.2667438
    10180.09751	-161.9615686
    10363.43854	-162.0367474
    10550.08148	-160.3216868
    10740.08583	-164.3862141
    10933.5121	-161.5718766
    11130.42193	-161.443985
    11330.87806	-161.5358625
    11534.94436	-161.7703865
    11742.68583	-160.8983236
    11954.16868	-162.6025896
    12169.46029	-160.4023453
    12388.62924	-164.137756
    12611.74537	-165.379528
    12838.87977	-163.5956685
    13070.1048	-162.2448727
    13305.49413	-162.7643937
    13545.12277	-161.9323755
    13789.06706	-163.1033658
    14037.40473	-161.9375793
    14290.21489	-161.8344954
    14547.57811	-161.4682056
    14809.57637	-163.641841
    15076.29316	-161.2772181
    15347.81344	-161.8367254
    15624.22375	-163.8937368
    15905.61213	-163.4045052
    16192.06824	-162.1718921
    16483.68336	-163.7274981
    16780.5504	-162.6159688
    17082.76394	-162.5689069
    17390.42027	-163.4016453
    17703.61741	-164.2673521
    18022.45515	-164.0711845
    18347.03509	-163.6379345
    18677.46062	-164.6454305
    19013.83704	-164.1375393
    19356.27151	-162.2678618
    19704.87315	-164.3286256
    20059.75301	-163.5123327
    20421.02417	-163.5551414
    20788.80174	-162.5823153
    21163.20288	-163.2599052
    21544.3469	-163.0973224
    21932.35523	-161.8897037
    22327.35149	-164.902143
    22729.46153	-164.157658
    23138.81348	-162.8473325
    23555.53775	-164.3067746
    23979.76713	-163.7059091
    24411.63677	-163.9764216
    24851.28427	-163.0963655
    25298.84972	-161.760677
    25754.4757	-162.1083328
    26218.3074	-161.2068699
    26690.4926	-162.4843046
    27171.18173	-162.8479923
    27660.52795	-161.8300854
    28158.68718	-161.8427446
    28665.81812	-162.1406767
    29182.08238	-161.1623182
    29707.64442	-161.6564092
    30242.6717	-162.1655339
    30787.3347	-162.0582672
    31341.80693	-162.7340918
    31906.26508	-164.2809079
    32480.88897	-162.659681
    33065.8617	-162.4699644
    33661.36964	-162.654158
    34267.60253	-163.8891935
    34884.75353	-164.9974573
    35513.01926	-164.5735966
    36152.5999	-163.630424
    36803.69923	-165.2187081
    37466.5247	-165.042907
    38141.28748	-164.5660422
    38828.20258	-163.7749291
    39527.48885	-164.8111397
    40239.36909	-165.0767971
    40964.07011	-164.9910649
    41701.82282	-164.4000895
    42452.86227	-167.5546349
    43217.42776	-165.9000342
    43995.76288	-165.0294028
    44788.11562	-164.9204892
    45594.73844	-164.5301561
    46415.88834	-167.0607835
    47251.82694	-167.8572846
    48102.82058	-166.133447
    48969.14041	-164.2463501
    49851.06245	-165.7078557
    50748.86768	-165.9278901
    51662.84216	-166.3563965
    52593.27709	-166.9150938
    53540.46892	-166.9672198
    54504.71945	-168.7749781
    55486.33588	-167.5086669
    56485.63098	-167.5884416
    57502.92314	-165.3553111
    58538.53648	-165.6251086
    59592.80096	-166.868997
    60666.05248	-167.3124287
    61758.63299	-166.7304423
    62870.8906	-167.2202427
    64003.1797	-168.2582305
    65155.86104	-168.1864497
    66329.30188	-169.0592121
    67523.8761	-168.1372196
    68739.96431	-170.1831888
    69977.95397	-169.3662685
    71238.2395	-166.7687762
    72521.22247	-169.5970032
    73827.31164	-167.0563767
    75156.92316	-169.0534012
    76510.48064	-169.8821676
    77888.41536	-168.7420031
    79291.16634	-168.4972862
    80719.18052	-170.0837521
    82172.91288	-169.7227838
    83652.82659	-171.3725896
    85159.39318	-171.2542111
    86693.09266	-168.2915231
    88254.41369	-170.4370879
    89843.85372	-169.5320001
    91461.91917	-169.4377285
    93109.12558	-172.6394491
    94785.99777	-170.4591872
    96493.07	-170.5637155
    98230.88618	-170.8296781
    100000	-172.3911459
    101800.9751	-172.3684401
    103634.3854	-172.8840901
    105500.8148	-173.6802282
    107400.8583	-172.4515294
    109335.121	-171.8523204
    111304.2193	-173.8805117
    113308.7806	-172.9526573
    115349.4436	-174.6552627
    117426.8583	-173.4780313
    119541.6868	-173.4991765
    121694.6029	-173.2980704
    123886.2924	-173.9761937
    126117.4537	-174.0980453
    128388.7977	-174.8660948
    130701.048	-174.4564286
    133054.9413	-175.4761949
    135451.2277	-174.4990728
    137890.6706	-173.0613005
    140374.0473	-174.8474831
    142902.1489	-174.2102321
    145475.7811	-174.6833429
    148095.7637	-176.6938002
    150762.9316	-175.4429741
    153478.1344	-175.5404007
    156242.2375	-175.3216906
    159056.1213	-175.7487216
    161920.6824	-174.4688443
    164836.8336	-175.302814
    167805.504	-174.128723
    170827.6394	-178.2797139
    173904.2027	-177.9338053
    177036.1741	-176.3921171
    180224.5515	-174.7857884
    183470.3509	-176.7246992
    186774.6062	-176.2900354
    190138.3704	-176.5022184
    193562.7151	-175.0917855
    197048.7315	-177.8902165
    200597.5301	-175.6687035
    204210.2417	-177.7699929
    207888.0174	-176.5879916
    211632.0288	-176.5505092
    215443.469	-176.8175345
    219323.5523	-179.6176346
    223273.5149	-177.0291822
    227294.6153	-176.2871382
    231388.1348	-177.3244914
    235555.3775	-178.6914469
    239797.6713	-177.8722391
    244116.3677	-176.5688431
    248512.8427	-177.5201603
    252988.4972	-177.1221382
    257544.757	-177.8219384
    262183.074	-178.3294004
    266904.926	-177.1240433
    271711.8173	-176.8194049
    276605.2795	-176.718615
    281586.8718	-177.2307137
    286658.1812	-177.3320602
    291820.8238	-177.6704566
    297076.4442	-177.9048479
    302426.717	-176.7551508
    307873.347	-176.2808087
    313418.0693	-177.6213657
    319062.6508	-178.6044237
    324808.8897	-178.598386
    330658.617	-178.3302491
    336613.6964	-176.4956511
    342676.0253	-177.7329427
    348847.5353	-177.0590373
    355130.1926	-176.7247127
    361525.999	-177.1323263
    368036.9923	-177.9663858
    374665.247	-178.2362896
    381412.8748	-178.7497444
    388282.0258	-177.5059476
    395274.8885	-176.7173149
    402393.6909	-178.5856671
    409640.7011	-178.0978389
    417018.2282	-177.5040994
    424528.6227	-178.5906164
    432174.2776	-177.3952862
    439957.6288	-177.2366201
    447881.1562	-177.5794798
    455947.3844	-177.2784523
    464158.8834	-177.3011132
    472518.2694	-178.5559375
    481028.2058	-176.9236468
    489691.4041	-178.3025488
    498510.6245	-177.7404116
    507488.6768	-177.7686413
    516628.4216	-176.5916527
    525932.7709	-179.2532624
    535404.6892	-177.3326368
    545047.1945	-177.7317429
    554863.3588	-177.7539169
    564856.3098	-177.8276139
    575029.2314	-178.4220543
    585385.3648	-177.3586582
    595928.0096	-178.1002521
    606660.5248	-178.0969233
    617586.3299	-178.262084
    628708.906	-177.8004081
    640031.797	-177.6790916
    651558.6104	-176.8574393
    663293.0188	-177.2222502
    675238.761	-179.2332472
    687399.6431	-179.243461
    699779.5397	-178.061637
    712382.395	-178.7304443
    725212.2247	-177.2538042
    738273.1164	-178.4883595
    751569.2316	-178.6105632
    765104.8064	-178.1773136
    778884.1536	-178.9574942
    792911.6634	-179.3209282
    807191.8052	-178.1027059
    821729.1288	-178.6871373
    836528.2659	-177.590186
    851593.9318	-177.906996
    866930.9266	-177.6852401
    882544.1369	-177.0598255
    898438.5372	-178.0341968
    914619.1917	-178.0441433
    931091.2558	-178.0671554
    947859.9777	-178.0143154
    964930.7	-177.9904798
    982308.8618	-178.0109589
    1000000	-177.9763228
    1018009.751	-176.7010187
    1036343.854	-177.3871434
    1055008.148	-177.8625871
    1074008.583	-178.5398885
    1093351.21	-178.8194408
    1113042.193	-178.6605678
    1133087.806	-177.8478528
    1153494.436	-178.8203805
    1174268.583	-178.5327674
    1195416.868	-177.9597793
    1216946.029	-178.4547136
    1238862.924	-178.5615216
    1261174.537	-177.8617004
    1283887.977	-177.4422108
    1307010.48	-178.3632721
    1330549.413	-177.3248485
    1354512.277	-178.1973328
    1378906.706	-177.50818
    1403740.473	-178.0978626
    1429021.489	-177.9278085
    1454757.811	-177.6439264
    1480957.637	-177.2701749
    1507629.316	-177.5936916
    1534781.344	-177.5310324
    1562422.375	-177.3846614
    1590561.213	-177.5955432
    1619206.824	-177.638341
    1648368.336	-177.6911553
    1678055.04	-177.7267788
    1708276.394	-177.6251804
    1739042.027	-177.9355698
    1770361.741	-177.0981794
    1802245.515	-178.3313511
    1834703.509	-179.0529418
    1867746.062	-178.1594715
    1901383.704	-178.8389118
    1935627.151	-176.8108294
    1970487.315	-178.2157909
    2005975.301	-177.0124745
    2042102.417	-177.830909
    2078880.174	-177.4575888
    2116320.288	-178.4654758
    2154434.69	-178.4412811
    2193235.523	-178.9133634
    2232735.149	-178.028219
    2272946.153	-177.886351
    2313881.348	-178.0861831
    2355553.775	-178.1352395
    2397976.713	-178.372332
    2441163.677	-178.2255784
    2485128.427	-177.7306919
    2529884.972	-178.8076653
    2575447.57	-178.166988
    2621830.74	-177.927233
    2669049.26	-178.2230023
    2717118.173	-179.1575662
    2766052.795	-178.8989159
    2815868.718	-178.959569
    2866581.812	-180.0264247
    2918208.238	-178.8612925
    2970764.442	-178.0855069
    3024267.17	-177.2242176
    3078733.47	-178.2214124
    3134180.693	-178.0642682
    3190626.508	-178.1843878
    3248088.897	-177.3588272
    3306586.17	-177.8909391
    3366136.964	-178.791884
    3426760.253	-178.1906575
    3488475.353	-177.8231935
    3551301.926	-178.8260293
    3615259.99	-178.7598172
    3680369.923	-178.2763269
    3746652.47	-177.7283941
    3814128.748	-179.5781511
    3882820.258	-178.347414
    3952748.885	-179.9054758
    4023936.909	-179.1338198
    4096407.011	-178.7833628
    4170182.282	-179.3622975
    4245286.227	-178.8263734
    4321742.776	-178.8989878
    4399576.288	-178.4614976
    4478811.562	-178.1597518
    4559473.844	-178.4418995
    4641588.834	-179.4470798
    4725182.694	-178.9177633
    4810282.058	-179.0405744
    4896914.041	-179.1764718
    4985106.245	-178.2605249
    5074886.768	-179.7396678
    5166284.216	-178.6319581
    5259327.709	-178.8937385
    5354046.892	-178.3591924
    5450471.945	-178.6762707
    5548633.588	-178.5821112
    5648563.098	-178.6295827
    5750292.314	-178.5808607
    5853853.648	-178.4224774
    5959280.096	-178.6448111
    6066605.248	-178.7028264
    6175863.299	-179.6411258
    6287089.06	-179.6610537
    6400317.97	-178.8135835
    6515586.104	-178.8065039
    6632930.188	-178.7549644
    6752387.61	-178.75022
    6873996.431	-178.6669562
    6997795.397	-178.6620508
    7123823.95	-178.2499248
    7252122.247	-178.2423552
    7382731.164	-178.4792906
    7515692.316	-180.4443646
    7651048.064	-180.434852
    7788841.536	-180.5224834
    7929116.634	-180.5126705
    8071918.052	-179.6612489
    8217291.288	-179.6539848
    8365282.659	-179.3242751
    8515939.318	-179.8391833
    8669309.266	-179.8315592
    8825441.369	-180.1234062
    8984385.372	-180.5457357
    9146191.917	-180.5385186
    9310912.558	-180.1786526
    9478599.777	-180.1736163
    9649307	-180.1925751
    9823088.618	-180.2319298
    10000000	-178.7616094
    10180097.51	-180.0382386
    10363438.54	-180.0339465
    10550081.48	-180.026701
    10740085.83	-180.4081881
    10933512.1	-181.1943714
    11130421.93	-181.1897805
    11330878.06	-181.1857524
    11534944.36	-180.9108056
    11742685.83	-180.4876974
    11954168.68	-180.1684955
    12169460.29	-180.4473958
    12388629.24	-180.7171801
    12611745.37	-179.7531169
    12838879.77	-179.759049
    13070104.8	-179.9533391
    13305494.13	-179.9525351
    13545122.77	-179.9247884
    13789067.06	-180.4851806
    14037404.73	-180.1693285
    14290214.89	-180.1244411
    14547578.11	-180.200438
    14809576.37	-179.8197475
    15076293.16	-179.9394554
    15347813.44	-180.0776884
    15624223.75	-180.6077376
    15905612.13	-180.7726875
    16192068.24	-179.9038925
    16483683.36	-179.7123445
    16780550.4	-180.579359
    17082763.94	-179.5450625
    17390420.27	-179.2836015
    17703617.41	-179.6459067
    18022455.15	-179.5450452
    18347035.09	-179.9089948
    18677460.62	-180.8619536
    19013837.04	-181.1759086
    19356271.51	-181.1583213
    19704873.15	-180.3107603
    20059753.01	-180.9120367
    20421024.17	-181.7024165
    20788801.74	-181.1326702
    21163202.88	-183.0905137
    21544346.9	-182.4744139
    21932355.23	-181.6588895
    22327351.49	-181.8766273
    22729461.53	-182.5580954
    23138813.48	-183.0456453
    23555537.75	-182.6963938
    23979767.13	-182.9081136
    24411636.77	-184.5531559
    24851284.27	-183.7159157
    25298849.72	-183.3049917
    25754475.7	-183.5796125
    26218307.4	-182.871161
    26690492.6	-183.8441367
    27171181.73	-183.1347682
    27660527.95	-184.1961631
    28158687.18	-183.0577893
    28665818.12	-184.7568757
    29182082.38	-185.1869512
    29707644.42	-184.8891509
    30242671.7	-184.2775759
    30787334.7	-184.7405515
    31341806.93	-184.6508166
    31906265.08	-186.2638469
    32480888.97	-182.8911007
    33065861.7	-184.4662864
    33661369.64	-184.5073924
    34267602.53	-184.1230687
    34884753.53	-183.9261174
    35513019.26	-184.0059435
    36152599.9	-185.5307545
    36803699.23	-183.3174704
    37466524.7	-185.1832052
    38141287.48	-184.458181
    38828202.58	-184.6781107
    39527488.85	-184.6846632
    40000000	-185.0593892
    

  • thanks for the reply Noel, 

    We intend to operate it in 20M - 1G region, in this region do you expect the output amplitude to go below 1vpp ?

  • I am guessing this may be possible, I don't have the power sweep data at low frequencies.

    I think you'd better reserve a buffer stage after LMX2594 in order to ensure you have sufficient voltage swing.

  • Ok Thanks Noel, 

    Just wish to confirm once more, the 10 pin ribbon cable for connecting the Pro board and LMX2594 would also be part of the aval kit purchased from digikey/mouser right ?

    I hope I don't have to procure that separately ?

    regards 

  • correct, the box comes with the ribbon cable.

  • Thanks Noel,

    Can you please suggest an suitable buffer that can be used at the output of LMX if operating at low frequency range for getting 1.8vpp ?

  • Hi Siddharth,

    Unfortunately, we don't have any buffer that can support 1GHz with 1.8Vpp output.