Part Number: LMK04828
Hello -
We've been using the LMK04828 for a few years now, successfully. Our current initialization procedure is:
#1) We currently check against LOS<0x184[1:0]> to point manually point the PLL1 towards <0x147[6:4]> the available reference.
#2) After PLL1 locks <0x182[1]>, we then put the PLL1 into automode <0x147[6:4]=4>.
#3) Ensure that PLL1 is locked <0x182[1]>
We recently noticed that step#3 wasn't locking. We found is that the LMK locked (as per step#2) but we moved into automode too quickly. Doing the register writes by hand worked every time. Adding a small SPI delay, seemed to fixed the issue as well.
Question: do we need to wait a small amount of time between getting a PLL1 lock and going into automode? experimentally, we've found that to be the case. If so, what's the recommended time?
Thanks.
Chris H