Part Number: LMK00105
Hello,
I'm looking for a device that would input SE clock (~2V) and fanout it to 5 loads.
Freq=10 MHz.
Zload= 50 Ohm.
Can you please advise whether LMK00105 is designed to work with these load and frequency?
If not, can you please advise which device supports these requirements.
If no such device exist with 5 outputs, 4 outputs is also acceptable.
Thanks,
David.