Hi,
I need to find a way to synchronize all our devices in the production system with our master clock. We have an interferometer (can it serve as a grand master clock?) and the client devices (at least 9 computers), the time synchronization accuracy must be within 100ns. Can you provide solutions (software or hardware) or is there any resource we can find? Our OS is Linux (Obuntu 18.04). The communication method is through Ethernet.
I did some research, to reach 100ns accuracy, we need IEEE 1588 protocol. The thing I'm not sure is when I look at industrial network protocol, there are 4 protocols. Base on my understanding, EtherCAT might be the one suits our problem? So if we choose EtherCAT, then we can define which master clock is the best?
Best,
Eddie