Part Number: LMK04832
Hello,
Is it possible to use DC coupling in LVDS levels between a SYSREF output (odd numbered output) of LMK04832 to another LMK04832's Clkin0 input?
The Datasheet states that it is not an option, but it does work on the lab, and I wonder if it may cause damage to any of the ICs?
I have to send a long period sync/sysref pulse such as a 1 pulse per second signal (1PPS).
This signal's transitions are too far apart to use AC coupling, (the slave LMK's output is metastable in this configuration).
Single ended DC is an option, but there is no way to ground the negative input of the slave LMK in my pcb.
what do you suggest I should do?
Thanks
Itamar