Other Parts Discussed in Thread: LMH1983
Hi all
Would you mind if we ask PLLatinum simulation with LMK03328?
Our customer will use LMK0328 and customer's configureation as follows;
<Customer's configuration>
LMH1983->27MHz->LMK03328->148.35MHz->FPGA
We simulated phase noise using PLLatinum.
1. Input phase noise from LMH1983
We refered to Figure 2. CLKout1 Phase Noise on the LMH1983's datasheet.
Offset frequency Phase noise
100Hz -115.0dB
1000Hz -125.0dB
10000Hz -135.0dB
100000Hz -146.0dB
1000000Hz -150.0dB
2. We inserted these Phase noises at PLLatinum using .txt file.(We also attach .sim data for PLLatinum)
100 -115.0 1000 -125.0 10000 -135.0 100000 -146.0 1000000 -150.0
(We compress the .sim file with .zip. Because the forum can't accept .sim file.)
20200826_LMK03328.zip
3. As the result, the phase noise at each offsets get worse 10dB.
If our procedure is not correct, could you give us advice?
Kind regards,
Hirotaka Matsumoto