This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCM9102: Provide input clock of PCIe interface for DSP c6678

Part Number: CDCM9102


Hi team,

When the output clock of CDCM9102 is LVPECL level, Voh min (2.12V) is slightly less than VIH min (2.135V) of LVPECL level of c6678 input interface. Can this be connected directly?

If use CDCE62002, it should be able to connect directly. However, CDCM9102 is dedicated to PCIe. I'm rather confused about which one to choose.

Best Regards,
Amy Luo