This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE6214: Clock generator that can supply clock to AM5728

Part Number: CDCE6214
Other Parts Discussed in Thread: AM5728, , CDCM9102

Dear TI Team

Our customer is looking for a clock generator to use on the board in AM5728.
CDCE6214 was selected because it meets the following specifications.
・PCIe support,
・4 outputs (3 outputs will be actually used)
・Power supply 3.3V

Also, since the CDCE6214 can output the same output format as the CDCM9102 installed in the AM5728EVM, we believe that the CDCE6214 can be used as a device that supplies a clock to the AM5728.

Is the above recognition correct?

Best Regards,

Y.Ottey