Part Number: CDCEL913
Other Parts Discussed in Thread: ADC3660,
I’m using a 12 MHz crystal oscillator and a CDCE(L)913 clock generator chip to drive the clock signals into an ADC3660. The CDCE(L)913 datasheet mentions an on-chip programmable load capacitance (default value of 10pF), and it says that external capacitors should ONLY be used for very fine adjustments; in my current design (and in past designs that used this clock generator chip), we have used two external 18pF capacitors, but I'm not sure if this is adversely impacting the output clock signals.
Application Report SCAA085 defines load capacitance as the on-chip programmable capacitance plus stray capacitance (plus, I assume, the external capacitors that I'm using). The crystal I am using has a specified load capacitance of 18pF.
The CDCE(L)913 datasheet also says that the device has an input capacitance of 1.5pF that must be added to the programmed load capacitance, and the two external capacitors should have an equivalent capacitance of 9pF; if I’m doing the math correctly, I believe that means that we should actually program the on-chip load capacitance to 7pf (rounded down from 7.5pF):
On-chip capacitance = 18pF – 1.5pF – 9pF = 7.5pF
Do you think that using the default value of 10pF instead of the “correct” value of 7.5pF will have any noticeable effect on the clock generator outputs? If such a small difference DOES have an effect, would it be better if I remove the external capacitors and program the on-chip capacitance to 16pF?