Part Number: LMX2572
We are considering a configuration with a frequency step of 1 MHz in the 6 GHz band, with SYNC=enable state. In case of integer division with phase comparison at 500 kHz, the loop bandwidth is reduced and phase noise is degraded due to the restriction of C1≥1500pF. So, we are considering fractional division, but PLLatinumSIM calculation shows that the largest spurious factor is MASH_Nonlinear. In order to suppress the spurious, we set the loop filter to a narrower bandwidth of about 10kHz and a smaler phase margin of about 45 degrees than in the automatic calculation. The order of the filter may be reduced. At first, I assumed to use 3rd Order MASH, but 2nd Order MASH seems to have a lower spurious. Let me ask you a few questions about the spurious.
(1) I heard before that LMX2572 does not use dithering, is it OK to use large fraction when SYNC=Enable?
(2) "?" of "N Divider Fractional Settings" instructs to check the spurious of large fraction by 100% randominzation. We want to keep the spurious below -70dBc at worst, but with the above setting, the MASH_Nonlinear spurious level is -73.3dBc with the best setting, and it degrades to nearly -50dBc with another seeds. The best seed value is searched by "Optimize Seeds for Spur Jitter", but will it be the same seed value at the time of Large Fraction setting and Simple Fraction?
(3) Because the Fden register of LMX2572 has 32 bits, I think the basic frequency of MASH_Linear spurious becomes less than 1Hz with the large fraction settings. Does the MASH_Linear spurious level of 100% randomization indicates a noise floor level?
(4) With Fpd=80MHz and Fnum/Fden=147/160 settings, the MASH_Linear spurious level does not change much with Randomization=0% and 100%.
I think the total spurious power of the MASH output will be constant regardless of the setting, and when the basic frequency of the spurious is changed from 500 kHz to 1 Hz, the spurious level would be 1/500,000. Is there any other restriction?
(5)In conclusion, which is recommended, simple fraction and large fraction?. In simple fraction, Fnum value is between 77 and 147, so, Fden becomes 80,40,32,20,16,8,5,4,2.
Moreover, if there is a point that should be reviced about above setting, could you give us advice?