Hi Team,
May I know the input impedance of Fin and Fin* pins? Thanks!
Best Regards!
Hao
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
May I know the input impedance of Fin and Fin* pins? Thanks!
Best Regards!
Hao
HI Noel
Can I understand in this way:
Almost all of input power will be absorbed by matching resistance and FIN pin just need a certain electrical level.
IF I have a external VCO, max output of VCO is very close but not up to the min required power level of FIN pin(-5dBm),
CAN I place a greater matching resistance near FIN pin and then use impedance mismatch to increase the FIN INPUT VOLTAGE LEVEL to avoid adding an amplifier?
Hi There,
At this frequency, Fin sensitivity is better than -20dBm, you can stick on 50Ω matching.