Part Number: LMK04826
Other Parts Discussed in Thread: LMK04832
Hi
In my custom Board, I am trying to Synchronize 5 LMK04826 devices with respect to input clock of 100 MHz.
I need to use Zero Delay Mode for all LMKs
I am having few limitations in my design
1. Inputs for all LMK's are given at OSCin pins. Clkin1, Clkin2, Clkin3 are left unconnected. So I can't use PLL1, I can only use the PLL2 in all the LMK's.
2. My input to LMK 1 is fixed. It was 100 MHz. I can't change it.
3. Outputs for each LMK are also fixed as shown in the below Block Diagram. (Clock outputs highlighted in Green indicate that they are fixed) .
4. Inputs to LMK2, LMK 3, LMK4, LMK 5 is not fixed. I can change them to get the Zero Delay Mode.
5. Between LMKs, I have only one Device Clock connection. So I can't give Sysref from first LMK as input to other LMKs.
In the Below attached Diagram,
Green -- These Frequencies are fixed and not changeable
Red -- Not Fixed. Can be changed to achieve Zero Delay Mode
So In this System, I need everything to be synchronized with respect to 100 MHz input Clock or I need all the outputs of 5 LMKs to be synchronized
My Hardware design is Fixed, I can't make any modifications.
I can't give sysref clocks from one LMK to other. I only have Device Clock connected from one LMK to other.
How to achieve Zero Delay mode in this.
What must be the OSCin Frequency for LMK 2, LMK3, LMK4, LMK5 ??
Can you help me with the configurations ??