This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2581E: Is N divider only for Fin?

Part Number: LMX2581E

In device block diagram, it seems to be that N divider is only for Fin source.

Could N divider, PLL_N, configuration not be used for OSCin source?

  • Hello Taikyon,

    The circuitry for the N-divider is hard-wired to the RFin/VCO mux, so the PLL_N configuration only works for the feedback path (not for OSCin). The OSCin path has its own divider, but this divider is integer-only (though some basic fractions like 2/3 are supported with the use of the multiplier). It turns out that putting a full fractional divider on the reference input is very challenging for performance and spur reasons; at this time I do not know of any device with a fractional input divider.

    Regards,