Part Number: CDCLVC1108
I have a customer looking into a minor change, and are considering moving from the 4-Ch (CDCLVC 1104) to the 8-Ch (CDCLVC 1108).
I didn't see any Electrical Characteristics variations between devices in the DS, so is it safe to assume 4-Ch and 8-Ch are electrically equivalent (in their max/min ratings as well), the only difference being the package and number of pins/supported channels?
Are they P2P replacements for the following? Any key electrical characteristics concerns...?
- IDT(now Renesas): 5PB1108PGG
BOMCROSS shows they are "P" - not P2P, but looking at the datasheet they are both TSSOP packages w/ 16-pins, and look like the pin-out is the same.
- ONSEMI: NB3V1108C
BOMCROSS says we don't have an option, but it looks like 16-pin TSSOP package with same pin-out.
Can you help me check the electrical characteristics for key concerns? They look P2P to me...
Thanks,
Darren