Part Number: LMH1983
In my application I only care about the clock outputs and do not use the TOF outputs. Can I drive the H-sync only with a generated H sync equivalent to NTSC (525i) and set V-sync and F-sync to 0 ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMH1983
In my application I only care about the clock outputs and do not use the TOF outputs. Can I drive the H-sync only with a generated H sync equivalent to NTSC (525i) and set V-sync and F-sync to 0 ?
Hi Jeff,
Only Hin signal is needed to lock the PLL. Vin (and Fin for interlace video input) is only needed to align the output TOF pulses.
Thanks and regards,
Amin