Part Number: SA555
Other Parts Discussed in Thread: TINA-TI
Dear TI,
I'm using the SA555 timer to generate a PWM frequency with the circuit shown below. The clock input is generated using another SA555 IC with Ra=Rb=12k and C=20nF.
To vary the PWM in the circuit below CONT (pin 5) is fed using a 0-5V dc signal driven using an-amp. Not matter what the dc level at CONT, the PWM remains fixed frequency. Is the source impedance from the op-amp too low, and can CONT only work when AC coupled?
Thanks, Rob