Other Parts Discussed in Thread: LMX2592,
Similar to Matthew Nickels61 (from E2E Clock & Timing Forum, "LMX2592: Reducing harmonic content of LMX2592 output"), I am using a LMX2592EVM as a tunable RF synthesizer. Specifically, I will tune the output from 150MHz up to 1.6GHz. In testing output frequencies between 100-490MHz, I observed strong odd harmonics of the output frequency. I have listed my configuration below. Is it typical of this type of frequency synthesizer to produce strong odd harmonics or harmonics, in general? If so, is there a way to reduce the harmonic levels significantly without a tunable filter? Also, do you expect that I will consistently see strong odd harmonics over my whole range (150MHz-1.6GHz) using the configuration below? Would you expect I would see even harmonics as well? Is there a different frequency synthesizer architecture that has similar or better performance without producing harmonics?
Configuration:
- Using on-board oscillator with Fpd=50MHz
- Output LO=150MHz to output LO=1.6GHz using channel divider and only output A (output B disabled)
- 4th order MASH
- Single-ended mode
- Fractional-N mode
Appreciate your insight.