Part Number: CDCE6214
Hi CTS team,
I need some clarification on the application note; for load capacitance, the formula given is below;
CL = CL1/2 + Cint_L1/2 + Cstray
CL is the load capacitance ; from the crystal spec, this is 18pF
CL1 is the external load capacitors – currently 10pF
CINT_L1 is the internal capacitance programmed in the device – form the settings this is 4.4pF
Cstray is approx.. to 3pF typically.
Using the formula ; 10/2 + 4.4/2 +3 = 10.2pF
Looking at the CINT_L1, which is programmed in IP_XO_CLOAD register;
- The description given is that the programmed value is the sum of the two internal load capacitors?
Does mean that I don’t halve as suggested by the formula?
- It appears that this programmed value also allows for the CSTRAY capacitance 3pF, given that the value to ‘0 ‘ would still include the 3pF capacitance – described in the TICs GUI.
With Regards,
Kris