Part Number: LMX2571
Other Parts Discussed in Thread: LMX2572LP
Hi PLL team,
Is it possible to generate a continuous phase FSK signal using LMX2571 or any other synthesizer TI offers?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello 0dBc,
We have two synthesizer products that support FSK: LMX2571, LMX2572LP
Please refer to section "7.3.13 FSK Modulation" of the LMX2571 datasheet, and section "7.3.14 FSK Modulation" of the LMX2572LP datasheet for descriptions on what these devices are capable of.
In both these devices FSK modulation is achieved by changing the output frequency by changing the N divider value.
The FSK SPI FAST mode may be of interest, however because we are still changing the N-divider this would be discrete changes to frequencies.
Thanks,
Vibhu
Hi There,
we don't have any specific modulation engine inside the chip, the way that we realize FSK modulation is by changing the N-divider.
to support bandwidth limited FSK modulation, user needs to pre-process the data before modulating the synthesizer. For example, GFSK with LMX2571/72 is possible as long as the raw data is pulse-shaped before feeding to the chip. See below appnote for the concept and implementation. I believe the same technique can be applied to CPFSK.
Hi,
Could you provide a clear answer to the following question:
Can I utilize the LMX2571 such that the phase stays continuous when changing the N-divider while doing FSK modulation? There is no mention of phase continuity on the datasheet or the app note (SNAA309).
Hello 0dBc,
Unfortunately, I think the answer is no. The phase will not stay continuous when you adjust the N divider.
Thanks,
Vibhu