Part Number: LMK05318
Other Parts Discussed in Thread: , LMK5C33216
Hi,
I have a primary and redundant GPS receiver producing a 1-PPS output which I am planning to feed into the inputs of the LMK05318 and assign the primary with a higher priority and set the device to Auto-Revertive.
My question is after a period of time where neither of the inputs are valid (holdover) and an input becomes valid, will the 1-PPS output gradually bring itself inline with the valid input or will it "snap" to the input signal immediately? Do I also have to use hitless switching for this? If not I will use the ZDM functionality.
Thanks