Part Number: LMH1983
The LMH1983 accepts standard video time signals in order to derive locked audio and video clocks. It also has the option to accept fixed 10MHz and 27MHz clocks and locks its internal PLLs to those. In addition, it has the option for User Defined Formats where custom reference signal parameters are specified.
I am trying to use the part in User Defined Format mode to lock to an18.5625MHz clock via the HIN input. This frequency is available from an FPGA based SDI receiver that does not have a reliable HSYNC output. This frequency is 148.5MHz / 8 and is 27MHz x 11/16.
Some questions ...
1) Is this user defined situation possible?
2) What is the maximum frequency that can be input via the HIM pin and into the R divider?
3) What is the optimal phase detector frequency is this case? I am currently using R=1100, N=1600 which provides 16.875kHz PD frequency.
4) How should User Auto Format low and high range registers be set in this case?
5) How should User Auto Format Lines per Frame be set in this case?
6) What User Auto Format Charge Pump Setting Should be used?
7) How should User Auto Format Miscellaneous settings be set?
8) Once configured correctly should I expect the PLL1 lock status in register 0x2 to be set.