Other Parts Discussed in Thread: TICSPRO-SW
Hi Support,
I'm trying to figure out how to set the VCO_PHASE_SYNC and INPIN_IGNORE bit fields in the LMX2594 registers.
Figure 27 in the datasheet shows two different cases of Category 1 SYNC depending on the value of the CHDIV. When CHDIV = 2, or 4, or 6, it states that SYNC mode is required but SYNC pulse is not required, does this mean in this mode VCO_PHASE_SYNC should be set to 1 and INPIN_IGNORE should be set to 1? And when CHDIV = 1, it states that SYNC mode is NOT required, meaning that VCO_PHASE_SYNC should be set to 0 and INPIN_IGNORE should be set to 1?
Any insight is highly appreciated.
Thanks,
Shant