Other Parts Discussed in Thread: LMX2594,
Hello,
Both LMK04832 and LMX2594 have the function of the control signal to generate SYSREF.
When LMK04832 worked at clock distribution mode, the rising edge of SYNC is used as the trigger.
While LMX2594 worked host mode, the rising edge of SysRefReq is used as the trigger.
If the trigger control is periodic signal, and the period is just equal to the( SYSREF period *pulse numbers), pulse number is configured by SYSREF_PULSE_CNT register. So the question is about the output of SYSREF, if the output of SYSREF is continuous pulses or the pulse trains with same interval time?
Could you please help to analyze?
Best regards
Kailyn