Part Number: LMK03000CEVAL
HI,
I see in the schematic of the LMK03000 evaluation board that the CLK,DATA and LE of the SPI bus are connected to big resistors (15K in series to 27K to GND).
Are these resistors required?
I am asking this because I looked at another evaluation board LMK04832 and I saw that in this evaluation board the signals are connected to 10 ohm serial resistor
Why is the difference ? If I use USB2ANY in both cases, shouldn't them have the same schematic?
Yuval