This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK05318: LMK05318 XO using clipped sine wave for input?

Part Number: LMK05318


Can LMK05318 XO using clipped sinewave for input?

About 0.8Vp-p

How to connect to LMK05318?

Thank You

  • Hi,

    As long as the XO input requirements are met (either LVCMOS or differential) then there's no problem.

    So for 0.8Vpp, it needs to be differential. What you can do is to add a AC-coupling cap in the path of XO_P and tie XO_N pin directly to ground. Make sure to select "differential" for XO in the software settings.

    Regards,
    Hao