Part Number: LMX2572LPEVM
Other Parts Discussed in Thread: LMX2572LP, TICSPRO-SW, USB2ANY, LMX2571
We want to use an LMX2572LP EVM board to demonstrate that we can set up a deterministic phase relationship between REF input and RF output. But it's not clear if the SYNC input on the EVM is set up to support this.
REF in = 49.92 MHz, RF out = 38.4 MHz. This is a fixed frequency application.
From Fig 159 of the data sheet, I conclude this will be a Category 3 process. Fig 160 suggests that the SYNC pin should be driven with a differential signal but it's not clear from the EVM schematic if this circuitry is in place.
Can I configure the EVM board to provide a deterministic relationship, given these frequencies?
Thank you
Bob