Other Parts Discussed in Thread: LMC555
Hi,
I am using the timer to generate a switching frequency for a high frquency transformer, see circuit diagram below. 2fw is connected to the clock input of a D-Flip-Flop where Qn is connected to its input D. So it halfs 2fsw to fsw.
I must know which switching frequency range is possible.
So I did the error calculation below, including propagation delay times and VIT und VI(TRIG) tolerances from the datasheet.
The frequency range is quite big. The measured switching frequency at room temperature is 268.12kHz. So it is very near to the caculated value of 278kHz.
I am wondering if VIT can have the max. value of 3.9V while VI(TRIG) has its smallest value of 1.26V.
Or is VI(TRIG)=2.06V (MAX) when VI(TRIG)=3.9V (MAX)?
Thanks a lot for your help in advance.