Part Number: LMK61E2
Hi Ti,
We bough two pieces of LMK61E2. The first one looks fine in recent frequent tests. The second one was soldered on the similar PCB.
However, the output of the second LML61E2 is unstable.
After the register value writing, two registers' values change back to their reset values automatically and unexpectedly.
The register R32 changes back to its rest value 0x00,this makes the denominator 0 in the application of integer N divider.
The register R23 changes back to its rest value 0x20, the required value is 0x28
Once I re-writer the correct value the those resisters, their values change again a few seconds or a few minutes later.
Do you have any idea or clue of the abnormal behavior?
Best Regards!
Wallace