Part Number: CDCE949-Q1
Hi team,
1) Why the EVM has AC coupling(C4) at the clock input even though it's LVCMOS input?
2) For Xin/CLK-pin on the IBIS model, which XTAL input or LVCMOS input is modeled? My customer want to simulate with LVCMOS input mode.
3) In LVCMOS clock input mode, the load capacitor setting should be set to 0pF? or don't care?
Regards,