This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: Is there any issue with using the category 3 sync with full VCO assist?

Part Number: LMX2594


Hi team,

customer is having a small issue with the LMX2594. When we tune a couple devices to 13040 MHz using auto calibration, and then synchronize them using Category 3 sync, everything syncs up. But when we use full VCO assist to tune the same output frequency, and then synchronize the same way, the devices don’t sync. They maintain the same phase as if the sync pin is muted. The register sets in the parts are identical in the two modes except for the Register 8 and 20 differences that are used to force the cal values for full assist.

 

Is there any issue with using category 3 sync with full vco assist?

Thanks,

Kevin