Part Number: LMX2592
Other Parts Discussed in Thread: LMX2594,
Hallo. I load by spi registers calculated in Tics, but no lmx working. HW design is ok, powers and ref in. Do I have send optional commands by spi ? BR
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
yes. attached
R64 0x400377 R62 0x3E0000 R61 0x3D0001 R59 0x3B0000 R48 0x3003FD R47 0x2F08FC R46 0x2E0F63 R45 0x2D0000 R44 0x2C0000 R43 0x2B0000 R42 0x2A0000 R41 0x290001 R40 0x280000 R39 0x278204 R38 0x26003C R37 0x254000 R36 0x240011 R35 0x23021F R34 0x22C3EA R33 0x212A0A R32 0x20210A R31 0x1F0201 R30 0x1E0034 R29 0x1D0084 R28 0x1C2924 R25 0x190000 R24 0x180509 R23 0x178842 R22 0x162300 R20 0x14012C R19 0x130965 R14 0x0E0420 R13 0x0D4000 R12 0x0C7001 R11 0x0B0018 R10 0x0A1158 R9 0x090302 R8 0x081084 R7 0x0728B2 R4 0x041943 R2 0x020500 R1 0x010808 R0 0x00001C
Hi Dim,
The Multiplier setting is not correct, there are input/output frequency requirement to the Multiplier.
Suggest set Multiplier = 1 but use Doubler = x2 to maintain 100MHz fpd. In general, we don't need FCAL_FAST and ACAL_FAST. Others look good. Make sure after Vcc power up, program all the registers once in descending order.