Other Parts Discussed in Thread: CDCE6214, CDCI6214, CDCEL913, LMK03318, CDCE913, CDCS503, USB2ANY, CLOCKPRO
Dears
Could our device support 74.25M / 148.5M input, and also same frequency output, with SSC function? thanks
Jun Shen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
And additional question, about the SSC modulation frequency? do we have this parameter? thanks
Hello Jun Shen,
The devices listed on the Original Question are CDCE6214, CDCI6214, CDCEL913 and LMK03318.
CDCE6214 has input and PLL supported for both 74.25MHz and 148.5MHz (See details in Table 4 for configuration details). I will have to check if SSC is capable at these frequencies.
CDCI6214 has removed the SSC support from CDCE6214.
CDCEL913 should support both frequencies with SSC functionality utilizing single-ended input and output.
LMK03318 does not support SSC but can support both of these output frequencies.
Will your device be a Clock Generator as well? Please take a look at our sorting tool found at ti.com when searching under the 'Product' and 'Clocks & timing' tabs. Hopefully this helps!
Aaron
Thanks, and the device number is CDCE913, currently customer just want use 1ch, with same input and output frequency, with the selectable SSC function, and do not need the I2C control, so want to know if we have some guide or reference schematic to use the CDCE913 in this way, like our CDCS503, very simple, but support higher input frequency.
thanks
Jun Shen
Hello Jun Shen,
Unfortunately, the SSC is selected through I2C on the CDCE913 while the CDCS503 has pins that can be used to select this functionality. If you would like to save an EEPROM image this could be done on start-up. I would recommend seeing the CDCE9xx family User's guide as well as CDCE9xx & CDCEx06 Programming Evaluation Module.
I have also asked about the CDCE6214 and this is also able to support these frequencies and SSC functionality. I would advise the use of the TICSPRO wizard for this device as it is incredibly helpful in finding settings of the PLL.
Hi Aaron
Thanks for the help, and currently we are working on CDCE913, seemed this device can be pro programed for the EEPROM once, like in the a assembly line. and after that the device can be setting by the PIN, or using the new setting in the EEPROM after power up, right?
By the way, do we have some programing tools to program the CDCE913, like the USB2ANY, USBTOGPIO?
Thanks
Jun Shen
Hello Shen,
We offer a Programmable EVM that can be used to accomplish programming EEPROM. Please see this CDCE(L)9xx and CDCEx06 Programming Evaluation Module as a reference. All that is required is a 2.0 USB cable as there is a built in MSP430. The user's program is TI ClockPro.
If you are looking for just a performance board please see the CDCE(L)9xx Performance Evaluation Module as this offers programmability but this is just to check performance.