Part Number: LMK04828BEVM
1. Using the chip dual PLL mode, the corresponding indicator will be on for the first time with the default configuration of the official website, and the reconfiguration lock indicator will not be on after the power is off.
2. How about the read lock indication status register status register?
3. Can't read
4. The software report requires other dll files
5. Only the first time is successfully configured, and the PLL cannot be locked later
6. There are corresponding indicators on the board