Part Number: LMX2594EVM
Other Parts Discussed in Thread: LMX2594, PLLATINUMSIM-SW, TICSPRO-SW
We are using the LMX2594 in a fast tuning application. In order to meet our settling time specification we are using it in full assist calibration mode. The reference frequency used depends on the output frequency. For frequencies below 7500 MHz we are using a 50 MHz reference. For frequencies above that we use a 100 MHz reference. The short term settling seems to be working as expected. That is, the output phase settles down in about 10 uS. This period is measured from the rising edge of the last SPI transfer to the output of our test setup.
The test setup consists of a microwave synthesizer set to 6 GHz, that is input to the LO port of a mixer. The RF port of the mixer is connected through a 10dB attenuator to the LMX2594 EVM. The IF port of the mixer is connected to an oscilloscope. We have conducted two types of tests. One is a large frequency change (6-9 GHz) and the other is a small one (6.0 to 6.1 GHz). In both cases the short term settling appears to be working well. However, we are seeing considerable phase drift for up to one mS before finally stopping.
O'Scope captures of the two cases are attached. the short term hop is below. The saved phase (lighter trace) was taken with a stock EVM. The darker trace was taken after a 220uF capacitor was added across the input power terminals. The top trace is just a trigger, the bottom trace is the SPI chip select signal.
The second scope capture shows the larger frequency step. Note the small negative "bump" about 3/4 of the way to the final value.
Is this behavior normal? If not, is there some setting or register value that could affect it (e.g. internal regulator bypass etc.)?
thanks
Fred Schader