Part Number: LMH1981
Other Parts Discussed in Thread: LMH1982,
I use the LMH1981 sync separator to pass HSOUT, VSOUT and FOUT to my FPGA. These signals are then fed through to the LMH1982. From time to time the LMH1982 loses reference, because there are glitches on the HSOUT signal, and more rarely, there is even a missing HSOUT pulse. The LMH1981 is being fed by a SDI digital to analog converter, 1V p-p (after terminator) through a 1uF ceramic AC-coupling capacitor at the pin of the LMH1981. The signal is PAL Black and burst.
The same circuit has worked fine in the past, so I'm wondering if in the last couple of years a batch change has happened to the LMH1981 which is causing this? Or is the AC-coupling capacitor material critical?
Kind regards,
Simon