Part Number: LMX2572
Hi Ti Experts,
On my own board, I am experiencing abnormal spur issue with LMX2572., conditions are,
1, OSC in = PFD = 100MHz, Single Ended, VCXO[CVHD950] sin-wave output.
2, 2572 output freq = 1200MHz on output A, INT mode, internal VCO = 4800M
unstable phase noise near 10MHz offset were noticed when measuring with SSA. When looking at 1210MHz on spectrum analyzer, it shows a batch of walking spurs. Here are video records.
I also measured frequency at 2400MHz, similar results as 1200M. However, when set pll as VCO output of 4800MHz, phase noise is stable and no walking spurs on spectrum analyzer. Base on above measurement, it seems rf divider contributes the walking spur, but this only occurs near 1200/2400MHz frequency range, no such abnormal issue at 600MHz.
I wonder if there is any furthure effors i can try on this issue.
Thanks in advance!
T.L.