Part Number: LMX2594EVM
Other Parts Discussed in Thread: LMX2594
I'm working on an application running at 3.2 GHz with a 10 MHz reference using TICSPRO. According to the automatically generated outputs (CHDIV etc.) the LMX2594 is operating in SYNC category 1 if I have followed the flowchart correctly. My understanding is that I must enable the VCO_PHASE_SYNC in this case but I do not need to provide a sync pulse to assert a deterministic phase on power-up. Can you confirm that this is correct?
I'm asking mainly because my test results do not demonstrate a deterministic phase relationship through power-up and I'm wondering if I have configured something incorrectly or if I have somehow misinterpreted the flow chart.
My test bench consists of sampling two 3.2 GHz signals simultaneously. The first signal is the output from the EVM (the signal from which I am looking for a deterministic phase on startup. The second signal is generated by a 3.2 frequency synthesizer that provides its reference to the EVM and if left running continously without perturbing its output in any way during the duration of the sample capture. Sample for sample, I monitor the baseband phase difference between these two signals which is very stable at the level of better than 1 degree over a period of minutes. Randomly during the capture, I power down the EVM, bring it back up, and reprogram it with TICSPRO and look to see if the phase difference continues on where it left off when the EVM was shutdown. In some cases, the EVM starts up in phase where it left off, more often though there is a significant difference in the phase difference before and after the powerdown event.
Can you offer any insight into why I am observing non-deterministic phase through a power cycle?
Chris