Part Number: LMK04826
Hello
After POR, Pin5 is set to RESET as default.
What is the programming sequence that does not use the RESET pin during external pull-up at Pin5?
Can I config the LMK04826 when external pull-up at Pin5?
Best Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMK04826
Hello
After POR, Pin5 is set to RESET as default.
What is the programming sequence that does not use the RESET pin during external pull-up at Pin5?
Can I config the LMK04826 when external pull-up at Pin5?
Best Regards
Hello Louis,
If the RESET pin is high, SPI programming will not take effect. The RESET pin must be held low or left floating to allow device programming.
If you have a microcontroller or other device which can pull the RESET pin low after POR, you can then configure 0x14A which contains the RESET_MUX and RESET_TYPE fields. You could, for instance, set 0x14A = 0x06, which configures the RESET pin as an open-drain output, guaranteeing that signals, noise, or pull-up configurations on the RESET pin do not trigger a reset.
Regards,