This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK03328: Jitter characteristic

Part Number: LMK03328
Other Parts Discussed in Thread: LMK05318B

Hi team,

Our customer is looking for the device which jitter is lower than LMK03328.

Use condition :I2C control,  Input(LVDS) 74.25MHz or 148.25MHz, Output(LVDS) 148.25MHz or 297MHz, VDD=3.3V, VDDO=1.8V

If there is some device, could you introduce?

Best regards.

teritama

  • Hi Teritama,

    What is the target jitter requirement and is this for pro audio/video? This is strange because I'm not aware of any application other than high speed Ethernet that requires better jitter than what LMK03328 can provide. 

    Technically the only device that has better jitter than LMK03328 is LMK05318B's first BAW APLL. However, that only supports Ethernet frequencies.

    Regards,
    Hao