I plan to use the LMK00334RTVRQ1 as a clock buffer for PCIe 2.0.
The datasheet lists the Output rise time 20% to 80% when using 250MHz input.(typ.225ps, Max.400ps)
Please teach me that the Output rise time 20% to 80% when using 100MHz input.
I am thinking the following as input.
3.3V differential LVDS clock. Freq:100MHz, Slew rate:4.95V/ns.
And, I thinking the following as output.
2 PCIe Gen HCSL clock.
Thanks.