Part Number: LMX2571EVM
Other Parts Discussed in Thread: LMX2571, USB2ANY
Hey E2E support,
I have a customer with a question regarding the LMX2571EVM,
In the LMX2571 datasheet it is stated that the supply voltage while working with the SPI digital interface is 3.3 volts.
However in the EVM schematic, a resistor divider (10k/12k) is used to convert the 3.3 logic from USB2ANY interface adapter down to 1.8V at LMX25731 SPI/Microwire input.
Is there a reason for this difference ?
Thank you for your help !
- Eyal