Part Number: LMX2594
Hello, I would like ask you the unclear explanation of the bit14 in the Register7: OUT_FORCE. There is description of the bit R0.9 "If disabled, also be sure to enable OUT_FORCE....If enabled, also be sure to disable OUT_FORCE" in the datasheet (page 46, table24, ver April 2019). It means the bit R7.14 must be always inverted value of R0.9. But in the default setting both bits have got value "0". I think, the description for OUT_FORCE is probably to strict, but I am not sure. Or is the Description correct and the default values shall be fixed during init-configuration?