Part Number: LMX2571
Other Parts Discussed in Thread: LMK03328
Hi all
Would you mind if we ask LMX2571?
<Question1>
Our customer's VC-TXCO(sine wave 57.6MHz) is Vpp=0.6V.
So, in case of single end, Vpp requires minimum 1.4V at least.
That's why, we consider using ditterential setting like as follows;
-IPBUF_SE_DIFF_SEL = 1
-IPBUFDIFF_TERM = 1
Is it possible to configure it?
If you have some notice in case of sine wave input, could you share us?
<Question2>
In relation to <Quesiton1>, if it is OK, how much of VOSCin's voltage does it require?
We assume that it requires minimum 0.15×2=0.3V at least.
Is it correct?
<Question3>
Just in case, how much is VT(bias voltage in case of differential clock)?1/2Vcc, right?
<Question4>
In relation to <Question3>, in case of differential clock setting, bias voltage adds to OSCin pins.
In case of single end setting, bias voltage doesn't add to OSCin pins, right?
If IPBUFDIFF_TERM Bit(R34) is on, does bias voltage adds to OSCin pins in spite of single end setting?
<Question5>
If you have block diagram of OSCin pins, could you share us?
We assmue that it is similar to LMK03328's one like as follows;
Kind regards,
Hirotaka Matsumoto