Other Parts Discussed in Thread: LMK03328
Hi all
Would you mind if we ask LMX2571?
We would like to confirm Voscin with Single ended input condtion.
<Question1>
How much is the VIL?
We assume that there is only the description of VIH, min=1.4V and max=3.3V.
<Question2>
On 6.5 Electrical Characteristics, there is the description Vosin's the condition with Single ended input.
Could you share us the test condtion for this as the reference?
Is input CMOS?
<Question3>
In relation to Question2, if the input reference is CMOS in case of test circuit, why is the min=1.4V?
We guess that it will be VCC×0.7.
Kind regards,
Hirotaka Matsumoto