Part Number: CDCE72010
Other Parts Discussed in Thread: CDCLVD110A,
Hello team,
I'd like to connect CDCLVD110A LVDS output to CDCE72010 PRI_REF pins with DC coupling.
Looking at the D/S, the CDCLVD110A VOS is 0.95 - 1.45V.
CDCE72010 Vicm is 1.0 - VCC-0.3V.
So, the minimum input level may violate the minimum output level of CDCLVD110A.
In this case, do you recommend to switch the connection to AC-coupling and then apply dc bias seperately?
Regards,
Itoh