Other Parts Discussed in Thread: CDCLVD1208
RE: CDCLVD1208 questions
1) I am not using the differential input 0, should I connect the inputs as follows:
INP0 - 1K pull-up to 2.5V supply rail ?
INN0 - 1K pull-down to ground?
2) The spec mentions ”low additive jitter: < 300 fs RMS in 10 KHz to 20 MHz”
I will use the chip with a 125.0MHz clock and a 312.50MHz clock and I need to know what kind of additive jitter I can expect at each of these rates?
The answer I got was:
The additive jitter spec is valid up to 800 MHz
You will get <300 fs additive jitter (from 10k-20MHz) with your applications frequencies 125 MHz and 312.5 MHz.
I want to know how much jitter the device is going to add at 125.0MHz and 312.50MHz which are the two clock rates I am going to operate the part at.
I will use one part for 125.0 Mhz and another part for 312.50 MHz to feed the reference clocks of an FPGA.
The way the spec is written “<300 fs additive jitter from 10k-20MHz” does it mean there is no jitter generated by the part above 20MHz?